This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ40Z80: Short circuit testing

Part Number: BQ40Z80
Other Parts Discussed in Thread: BQSTUDIO

Hello shirish,

Thanks for your feedback.

Now I we are doing the short circuit testing on our custom BMS board ( by connecting pack + and pack- pin toghether)  by shorting these still my pack voltage is not cutting off. Also I checked that on the bqstudio and I am not able to see that bq40z80 chip identify any short circuit. What could be the reason for that?

Regards,

Hrishikesh.

  • Hello Hrishikesh,

    Can you share a scope capture of the short circuit event current and your .gg file settings so we can review if the gauge should have disabled the FETs? Without any data it is not clear if the short circuit event caused a current high enough to trip a protection.

    Sincerely,

    Wyatt Keller

  • Dear Wyatt,

    Here is the attached .gg and log file of that testing. Because I couldn't able to capture that on the scope. Also we observed one strange behavior on the BMS.The current reading twice dropped down to -3.0Amps --- I was not doing anything at either of those times when this happened and there is no load connected to the battery – only my Fluke DVM reading the volts. I also attached image of that for your reference.

    Please have look and let me know.

    Regards,

    Hrishikesh.

    1732.BATTERY.zip

  • Hello Hrishikesh,

    The gauge CC input is very sensitive, removing or connecting a external piece of equipment can cause interference in the measurement. If nothing is connected to the the SRN and SRP pins and there is no EMI/RF interference then I would not expect any fluctuations in current. Were these spikes not at the time of the short circuit event?

    I don't see any indication of a short circuit event in the log, we would need to see the actual short circuit event to verify the gauge operation. Also it looks like you have disabled reserved bits associated with hardware protection, make sure you leave the reserved bits at the default value for enabled protections otherwise you will not see alignment with the ASCD/ASCC and the FET operation and may cause the gauge to not behave as expected.

    Sincerely,

    Wyatt Keller

  • Dear Wyatt,

    We again tried to be logged in the condition. Could you please have look at that?

    Regards,

    Hrishikesh.Battery-short.zip 

  • Hello Hrishikesh,

    The log shows that your short circuit is only about 23A, this would only trip the lowest ASCD threshold we have available and it is 22.2A which is within the possible error margin for hardware protections.

    Sincerely,

    Wyatt Keller

  • Dear Wyatt,

    We again did this short circuit testing on the BMS board & we observed some interesting. result on that

    We did short circuit 3 times on the BMS board. first time it cut off and as soon as we release the short circuit pack voltage come backs.

    Now did this same short circuit 2 more times but now this time it remains turned off only. We couldn't be able to understand this phenomenon.

    I have attached our testing results for your reference please have a look and let me know.

    Also, as you mentioned earlier that. "Your short circuit is only about 23A, this would only trip the lowest ASCD threshold we have available, and it is 22.2A which is within the possible error margin for hardware protections."

    Can we reduce the short circuit detection current? any other parameter? Please help us with this.

    Regards,

    Hrishikesh. 

    Tue Jul 25 10:41:32 CDT 2023
    
    Device Version Info = 4800_0_04
    BQZ Device Name = bq40z80
    BQZ Firmware Version = V0_04_BLD5
    
    Design Capacity = 3450
    Design Voltage = 21600
    Specification Info = 0x0031
    Manufacturer Date = 1980-1-1
    Serial Number = 0x0001
    Manufacturer Name = Texas Instruments
    Device Name = bq40z80
    Device Chemistry = LION
    
    Sample,DateTime,ElapsedTime,ManufAccess,RemCapAlarm,RemTimeAlarm,BattMode,@Rate(@),@TimeFull,@TimeEmpty,@RateOK,Temperature,Voltage,Current,AvgCurr,MaxErr,RSOC,ASOC,RemCap,FullChgCap,RunTimeEmty,AvgTimeEmty,AvgTimeFull,ChgCurr,ChgVolt,BattStat,CycleCnt,MaxTurboPwr,SusTurboPwr,MaxTurboCurr,SusTurboCurr,SoH,OpStatA,OpStatB,TempRange,ChgStat,GaugeStat,ITStat,MfgStat,SafetyAlertAB,SafetyStatAB,SafetyAlertCD,SafetyStatCD,PFAlertAB,PFStatAB,PFAlertCD,PFStatCD,CellVolt1,CellVolt2,CellVolt3,CellVolt4,CellVolt5,CellVolt6,CellVolt7,vBAT,vPACK,CellCurr1,CellCurr2,CellCurr3,CellCurr4,CellCurr5,CellCurr6,CellCurr7,CellPower1,CellPower2,CellPower3,CellPower4,CellPower5,CellPower6,CellPower7,Power,AvgPow,IntTemp,TS1Temp,TS2Temp,TS3Temp,TS4Temp,CellTemp,FETTemp,GaugeTemp,FltRemQ,FltRemE,FltFullChgQ,FltFullChgE,NoLoadRemCap,TrueRemQ,TrueRemE,InitialQ,InitialE,TrueFullChgQ,TrueFullChgE,T_sim,T_ambient,RaScale1,RaScale2,RaScale3,RaScale4,RaScale5,RaScale6,RaScale7,CompRes1,CompRes2,CompRes3,CompRes4,CompRes5,CompRes6,CompRes7,PackGrid,LStatus,CellGrid1,CellGrid2,CellGrid3,CellGrid4,CellGrid5,CellGrid6,CellGrid7,StateTime,DOD0_1,DOD0_2,DOD0_3,DOD0_4,DOD0_5,DOD0_6,DOD0_7,DOD0 Passed Q,DOD0 Passed E,DOD0 Time,DODEOC_1,DODEOC_2,DODEOC_3,DODEOC_4,DODEOC_5,DODEOC_6,DODEOC_7,QMax1,QMax2,QMax3,QMax4,QMax5,QMax6,QMax7,QMaxDOD0_1,QMaxDOD0_2,QMaxDOD0_3,QMaxDOD0_4,QMaxDOD0_5,QMaxDOD0_6,QMaxDOD0_7,QMaxPassedQ,QMaxTime,Tk,Ta,RawDOD_1,RawDOD_2,RawDOD_3,RawDOD_4,RawDOD_5,RawDOD_6,RawDOD_7,CBTime1,CBTime2,CBTime3,CBTime4,CBTime5,CBTime6,CBTime7,CBDOD_1,CBDOD_2,CBDOD_3,CBDOD_4,CBDOD_5,CBDOD_6,CBDOD_7,CBTotalDODChg,SOH_FC_Q,SOH_FC_E,LogRowTime(ms),LogStatus
    1,2023-07-25 10:41:36,4.015,0x0107,1000,10,0x6001,0,65535,65535,1,25.0,23940,0,0,1,100,662,22813,22857,65535,65535,65535,30552,25200,0x48C0,3,-1843,-15968,-1024,-6900,78,0x0107,0x0000,0x10,0x0004,0x50,0x0814,0x01B8,0x0000,0x0000,0x0000,0x0000,0xFF3F,0x0000,0x007F,0x0000,3990,3990,3990,3990,3990,3991,0,24340,23220,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,23.0,25.0,25.3,-273.2,-273.2,25.0,25.3,25.0,22813,4086,22857,4191,2701,22813,4086,44,105,22857,4191,25.0,25.0,1000,1000,1000,1000,1000,1000,0,0,0,0,0,0,0,0,0,14,0,0,0,0,0,0,0,88,2464,2464,2464,2464,2448,2448,0,0,0,0,1344,2240,1728,1488,1000,1920,0,3188,3197,3196,3179,3176,3204,4400,0,0,0,0,0,0,0,0,0,0.57,11291,2464,2464,2464,2464,2448,2448,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,2704,5877,1275,SUCCESS
    2,2023-07-25 10:41:40,8.020,0x0107,1000,10,0x6001,0,65535,65535,1,25.0,23941,0,0,1,100,662,22813,22857,65535,65535,65535,30552,25200,0x48C0,3,-1843,-15968,-1024,-6900,78,0x0107,0x0000,0x10,0x0004,0x50,0x0814,0x01B8,0x0000,0x0000,0x0000,0x0000,0xFF3F,0x0000,0x007F,0x0000,3990,3990,3990,3990,3991,3991,0,24341,23220,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,23.0,25.0,25.3,-273.2,-273.2,25.0,25.3,25.0,22813,4086,22857,4191,2701,22813,4086,44,105,22857,4191,25.0,25.0,1000,1000,1000,1000,1000,1000,0,0,0,0,0,0,0,0,0,14,0,0,0,0,0,0,0,92,2464,2464,2464,2464,2448,2448,0,0,0,0,1344,2240,1728,1488,1000,1920,0,3188,3197,3196,3179,3176,3204,4400,0,0,0,0,0,0,0,0,0,0.57,11291,2464,2464,2464,2464,2448,2448,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,2704,5877,1302,SUCCESS
    3,2023-07-25 10:41:44,12.032,0x0107,1000,10,0x6001,0,65535,65535,1,25.0,23941,0,0,1,100,662,22813,22857,65535,65535,65535,30552,25200,0x48C0,3,-1843,-15968,-1024,-6900,78,0x0107,0x0000,0x10,0x0004,0x50,0x0814,0x01B8,0x0000,0x0000,0x0000,0x0000,0xFF3F,0x0000,0x007F,0x0000,3990,3990,3990,3990,3991,3991,0,24341,23221,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,23.0,25.0,25.3,-273.2,-273.2,25.0,25.3,25.0,22813,4086,22857,4191,2701,22813,4086,44,105,22857,4191,25.0,25.0,1000,1000,1000,1000,1000,1000,0,0,0,0,0,0,0,0,0,14,0,0,0,0,0,0,0,96,2464,2464,2464,2464,2448,2448,0,0,0,0,1344,2240,1728,1488,1000,1920,0,3188,3197,3196,3179,3176,3204,4400,0,0,0,0,0,0,0,0,0,0.57,11291,2464,2464,2464,2464,2448,2448,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,2704,5877,1302,SUCCESS
    4,2023-07-25 10:41:48,16.038,0x0107,1000,10,0x6001,0,65535,65535,1,25.0,23941,0,0,1,100,662,22813,22857,65535,65535,65535,30552,25200,0x48C0,3,-1843,-15968,-1024,-6900,78,0x0107,0x0000,0x10,0x0004,0x50,0x0814,0x01B8,0x0000,0x0000,0x0000,0x0000,0xFF3F,0x0000,0x007F,0x0000,3990,3990,3990,3990,3991,3992,0,24341,23221,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,23.0,25.0,25.3,-273.2,-273.2,25.0,25.3,25.0,22813,4086,22857,4191,2701,22813,4086,44,105,22857,4191,25.0,25.0,1000,1000,1000,1000,1000,1000,0,0,0,0,0,0,0,0,0,14,0,0,0,0,0,0,0,100,2464,2464,2464,2464,2448,2448,0,0,0,0,1344,2240,1728,1488,1000,1920,0,3188,3197,3196,3179,3176,3204,4400,0,0,0,0,0,0,0,0,0,0.57,11291,2464,2464,2464,2464,2448,2448,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,2704,5877,1316,SUCCESS
    5,2023-07-25 10:41:52,20.042,0x0107,1000,10,0x6001,0,65535,65535,1,25.0,23941,0,0,1,100,662,22813,22857,65535,65535,65535,30552,25200,0x48C0,3,-1843,-15968,-1024,-6900,78,0x0107,0x0000,0x10,0x0004,0x50,0x0814,0x01B8,0x0000,0x0000,0x0000,0x0000,0xFF3F,0x0000,0x007F,0x0000,3989,3990,3990,3990,3990,3991,0,24340,23222,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,23.0,25.0,25.3,-273.2,-273.2,25.0,25.3,25.0,22813,4086,22857,4191,2701,22813,4086,44,105,22857,4191,25.0,25.0,1000,1000,1000,1000,1000,1000,0,0,0,0,0,0,0,0,0,14,0,0,0,0,0,0,0,104,2464,2464,2464,2464,2448,2448,0,0,0,0,1344,2240,1728,1488,1000,1920,0,3188,3197,3196,3179,3176,3204,4400,0,0,0,0,0,0,0,0,0,0.57,11291,2464,2464,2464,2464,2448,2448,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,2704,5877,1313,SUCCESS
    6,2023-07-25 10:41:56,24.049,0x0107,1000,10,0x6001,0,65535,65535,1,25.0,23941,0,0,1,100,662,22813,22857,65535,65535,65535,30552,25200,0x48C0,3,-1843,-15968,-1024,-6900,78,0x0107,0x0000,0x10,0x0004,0x50,0x0814,0x01B8,0x0000,0x0000,0x0000,0x0000,0xFF3F,0x0000,0x007F,0x0000,3990,3990,3990,3991,3991,3991,0,24340,23226,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,22.9,25.0,25.3,-273.2,-273.2,25.0,25.3,25.0,22813,4086,22857,4191,2701,22813,4086,44,105,22857,4191,25.0,25.0,1000,1000,1000,1000,1000,1000,0,0,0,0,0,0,0,0,0,14,0,0,0,0,0,0,0,108,2464,2464,2464,2464,2448,2448,0,0,0,0,1344,2240,1728,1488,1000,1920,0,3188,3197,3196,3179,3176,3204,4400,0,0,0,0,0,0,0,0,0,0.57,11291,2464,2464,2464,2464,2448,2448,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,2704,5877,1346,SUCCESS
    7,2023-07-25 10:42:00,28.058,0x0107,1000,10,0x6001,0,65535,65535,1,25.0,23941,0,0,1,100,662,22813,22857,65535,65535,65535,30552,25200,0x48C0,3,-1843,-15968,-1024,-6900,78,0x0107,0x0000,0x10,0x0004,0x50,0x0814,0x01B8,0x0000,0x0000,0x0000,0x0000,0xFF3F,0x0000,0x007F,0x0000,3990,3990,3990,3990,3991,3991,0,24340,23221,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,23.0,25.0,25.3,-273.2,-273.2,25.0,25.3,25.0,22813,4086,22857,4191,2701,22813,4086,44,105,22857,4191,25.0,25.0,1000,1000,1000,1000,1000,1000,0,0,0,0,0,0,0,0,0,14,0,0,0,0,0,0,0,112,2464,2464,2464,2464,2448,2448,0,0,0,0,1344,2240,1728,1488,1000,1920,0,3188,3197,3196,3179,3176,3204,4400,0,0,0,0,0,0,0,0,0,0.57,11291,2464,2464,2464,2464,2448,2448,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,2704,5877,1531,SUCCESS
    8,2023-07-25 10:42:04,32.073,0x0107,1000,10,0x6001,0,65535,65535,1,25.0,23941,0,0,1,100,662,22813,22857,65535,65535,65535,30552,25200,0x48C0,3,-1843,-15968,-1024,-6900,78,0x0107,0x0000,0x10,0x0004,0x50,0x0814,0x01B8,0x0000,0x0000,0x0000,0x0000,0xFF3F,0x0000,0x007F,0x0000,3990,3990,3990,3990,3991,3991,0,24341,23222,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,22.9,25.0,25.3,-273.2,-273.2,25.0,25.3,25.0,22813,4086,22857,4191,2701,22813,4086,44,105,22857,4191,25.0,25.0,1000,1000,1000,1000,1000,1000,0,0,0,0,0,0,0,0,0,14,0,0,0,0,0,0,0,116,2464,2464,2464,2464,2448,2448,0,0,0,0,1344,2240,1728,1488,1000,1920,0,3188,3197,3196,3179,3176,3204,4400,0,0,0,0,0,0,0,0,0,0.57,11291,2464,2464,2464,2464,2448,2448,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,2704,5877,1344,SUCCESS
    9,2023-07-25 10:42:08,36.082,0x0107,1000,10,0x6001,0,65535,65535,1,25.0,23941,0,0,1,100,662,22813,22857,65535,65535,65535,30552,25200,0x48C0,3,-1843,-15968,-1024,-6900,78,0x0107,0x0000,0x10,0x0004,0x50,0x0814,0x01B8,0x0000,0x0000,0x0000,0x0000,0xFF3F,0x0000,0x007F,0x0000,3990,3990,3990,3990,3991,3991,0,24339,23221,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,22.9,25.0,25.3,-273.2,-273.2,25.0,25.3,25.0,22813,4086,22857,4191,2701,22813,4086,44,105,22857,4191,25.0,25.0,1000,1000,1000,1000,1000,1000,0,0,0,0,0,0,0,0,0,14,0,0,0,0,0,0,0,120,2464,2464,2464,2464,2448,2448,0,0,0,0,1344,2240,1728,1488,1000,1920,0,3188,3197,3196,3179,3176,3204,4400,0,0,0,0,0,0,0,0,0,0.57,11291,2464,2464,2464,2464,2448,2448,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,2704,5877,1445,SUCCESS
    10,2023-07-25 10:42:12,40.084,0x0107,1000,10,0x6001,0,65535,65535,1,25.0,23941,0,0,1,100,662,22813,22857,65535,65535,65535,30552,25200,0x48C0,3,-1843,-15968,-1024,-6900,78,0x0107,0x0000,0x10,0x0004,0x50,0x0814,0x01B8,0x0000,0x0000,0x0000,0x0000,0xFF3F,0x0000,0x007F,0x0000,3990,3990,3990,3990,3991,3991,0,24339,23222,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,22.9,25.0,25.2,-273.2,-273.2,25.0,25.2,25.0,22813,4086,22857,4191,2701,22813,4086,44,105,22857,4191,25.0,25.0,1000,1000,1000,1000,1000,1000,0,0,0,0,0,0,0,0,0,14,0,0,0,0,0,0,0,124,2464,2464,2464,2464,2448,2448,0,0,0,0,1344,2240,1728,1488,1000,1920,0,3188,3197,3196,3179,3176,3204,4400,0,0,0,0,0,0,0,0,0,0.57,11291,2464,2464,2464,2464,2448,2448,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,2704,5877,1379,SUCCESS
    11,2023-07-25 10:42:16,44.084,0x0107,1000,10,0x6001,0,65535,65535,1,25.0,23941,0,0,1,100,662,22813,22857,65535,65535,65535,30552,25200,0x48C0,3,-1843,-15968,-1024,-6900,78,0x0107,0x0000,0x10,0x0004,0x50,0x0814,0x01B8,0x0000,0x0000,0x0000,0x0000,0xFF3F,0x0000,0x007F,0x0000,3990,3990,3989,3991,3991,3991,0,24340,23223,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,22.9,25.0,25.3,-273.2,-273.2,25.0,25.3,25.0,22813,4086,22857,4191,2701,22813,4086,44,105,22857,4191,25.0,25.0,1000,1000,1000,1000,1000,1000,0,0,0,0,0,0,0,0,0,14,0,0,0,0,0,0,0,128,2464,2464,2464,2464,2448,2448,0,0,0,0,1344,2240,1728,1488,1000,1920,0,3188,3197,3196,3179,3176,3204,4400,0,0,0,0,0,0,0,0,0,0.57,11291,2464,2464,2464,2464,2448,2448,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,2704,5877,1345,SUCCESS
    12,2023-07-25 10:42:20,48.093,0x0107,1000,10,0x6001,0,65535,65535,1,25.0,23941,0,0,1,100,662,22813,22857,65535,65535,65535,30552,25200,0x48C0,3,-1843,-15968,-1024,-6900,78,0x0107,0x0000,0x10,0x0004,0x50,0x0814,0x01B8,0x0000,0x0000,0x0000,0x0000,0xFF3F,0x0000,0x007F,0x0000,3990,3990,3989,3990,3991,3992,0,24340,23223,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,22.9,25.0,25.2,-273.2,-273.2,25.0,25.2,25.0,22813,4086,22857,4191,2701,22813,4086,44,105,22857,4191,25.0,25.0,1000,1000,1000,1000,1000,1000,0,0,0,0,0,0,0,0,0,14,0,0,0,0,0,0,0,132,2464,2464,2464,2464,2448,2448,0,0,0,0,1344,2240,1728,1488,1000,1920,0,3188,3197,3196,3179,3176,3204,4400,0,0,0,0,0,0,0,0,0,0.57,11291,2464,2464,2464,2464,2448,2448,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,2704,5877,1435,SUCCESS
    13,2023-07-25 10:42:25,52.107,0x0107,1000,10,0x6001,0,65535,65535,1,25.0,23941,0,0,1,100,662,22813,22857,65535,65535,65535,30552,25200,0x48C0,3,-1843,-15968,-1024,-6900,78,0x0107,0x0000,0x10,0x0004,0x50,0x0814,0x01B8,0x0000,0x0000,0x0000,0x0000,0xFF3F,0x0000,0x007F,0x0000,3990,3990,3990,3990,3991,3992,0,24339,23220,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,23.0,25.0,25.2,-273.2,-273.2,25.0,25.2,25.0,22813,4086,22857,4191,2701,22813,4086,44,105,22857,4191,25.0,25.0,1000,1000,1000,1000,1000,1000,0,0,0,0,0,0,0,0,0,14,0,0,0,0,0,0,0,136,2464,2464,2464,2464,2448,2448,0,0,0,0,1344,2240,1728,1488,1000,1920,0,3188,3197,3196,3179,3176,3204,4400,0,0,0,0,0,0,0,0,0,0.57,11291,2464,2464,2464,2464,2448,2448,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,2704,5877,1453,SUCCESS
    14,2023-07-25 10:42:29,56.119,0x6101,1000,10,0x6081,0,0,0,0,25.0,23935,0,0,100,0,0,0,3450,0,0,0,0,0,0x0040,3,0,0,0,0,0,0x6101,0x0100,0x08,0x0004,0x50,0x0814,0x01B8,0x0000,0x0000,0x0000,0x0000,0xFF3F,0x0000,0x007F,0x0000,3989,3990,3989,3990,3990,3990,0,24336,1,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,23.3,25.0,25.3,-273.2,-273.2,25.0,25.3,25.0,22810,4089,22857,4201,2698,22810,4089,47,112,22857,4201,25.0,25.0,1000,1000,1000,1000,1000,1000,0,0,0,0,0,0,0,0,0,14,0,0,0,0,0,0,0,0,2496,2480,2480,2480,2464,2464,0,0,0,0,1344,2240,1728,1488,1000,1920,0,3188,3197,3196,3179,3176,3204,4400,0,0,0,0,0,0,0,0,0,0.57,11291,2496,2480,2480,2480,2464,2464,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,2704,5877,1389,SUCCESS
    15,2023-07-25 10:42:33,60.124,0x6101,1000,10,0x6001,0,65535,65535,1,25.0,23938,0,0,1,100,662,22810,22857,65535,65535,65535,30552,25200,0x48C0,3,-1843,-15961,-1024,-6900,78,0x6101,0x0000,0x10,0x0004,0x50,0x0814,0x01B8,0x0000,0x0000,0x0000,0x0000,0xFF3F,0x0000,0x007F,0x0000,3989,3989,3989,3990,3990,3991,0,24336,10,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,23.0,25.1,25.3,-273.2,-273.2,25.1,25.3,25.1,22810,4089,22857,4201,2698,22810,4089,47,112,22857,4201,25.0,25.0,1000,1000,1000,1000,1000,1000,0,0,0,0,0,0,0,0,0,14,0,0,0,0,0,0,0,4,2496,2480,2480,2480,2464,2464,0,0,0,0,1344,2240,1728,1488,1000,1920,0,3188,3197,3196,3179,3176,3204,4400,0,0,0,0,0,0,0,0,0,0.57,11291,2496,2480,2480,2480,2464,2464,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,2704,5877,1433,SUCCESS
    16,2023-07-25 10:42:37,64.129,0x0107,1000,10,0x6001,0,65535,65535,1,25.1,23939,0,0,1,100,662,22810,22857,65535,65535,65535,30552,25200,0x48C0,3,-1843,-15961,-1024,-6900,78,0x0107,0x0000,0x10,0x0004,0x50,0x0814,0x01B8,0x0000,0x0000,0x0000,0x0000,0xFF3F,0x0000,0x007F,0x0000,3989,3990,3989,3990,3990,3991,0,24337,23217,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,23.0,25.1,25.3,-273.2,-273.2,25.1,25.3,25.1,22810,4089,22857,4201,2698,22810,4089,47,112,22857,4201,25.0,25.0,1000,1000,1000,1000,1000,1000,0,0,0,0,0,0,0,0,0,14,0,0,0,0,0,0,0,8,2496,2480,2480,2480,2464,2464,0,0,0,0,1344,2240,1728,1488,1000,1920,0,3188,3197,3196,3179,3176,3204,4400,0,0,0,0,0,0,0,0,0,0.57,11291,2496,2480,2480,2480,2464,2464,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,2704,5877,1446,SUCCESS
    17,2023-07-25 10:42:41,68.143,0x0107,1000,10,0x6001,0,65535,65535,1,25.1,23939,0,0,1,100,662,22810,22857,65535,65535,65535,30552,25200,0x48C0,3,-1843,-15961,-1024,-6900,78,0x0107,0x0000,0x10,0x0004,0x50,0x0814,0x01B8,0x0000,0x0000,0x0000,0x0000,0xFF3F,0x0000,0x007F,0x0000,3989,3990,3989,3990,3990,3991,0,24339,23218,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,23.0,25.1,25.3,-273.2,-273.2,25.1,25.3,25.1,22810,4089,22857,4201,2698,22810,4089,47,112,22857,4201,25.0,25.0,1000,1000,1000,1000,1000,1000,0,0,0,0,0,0,0,0,0,14,0,0,0,0,0,0,0,12,2496,2480,2480,2480,2464,2464,0,0,0,0,1344,2240,1728,1488,1000,1920,0,3188,3197,3196,3179,3176,3204,4400,0,0,0,0,0,0,0,0,0,0.57,11291,2496,2480,2480,2480,2464,2464,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,2704,5877,1450,SUCCESS
    18,2023-07-25 10:42:45,72.143,0x0107,1000,10,0x6001,0,65535,65535,1,25.1,23939,0,0,1,100,662,22810,22857,65535,65535,65535,30552,25200,0x48C0,3,-1843,-15961,-1024,-6900,78,0x0107,0x0000,0x10,0x0004,0x50,0x0814,0x01B8,0x0000,0x0000,0x0000,0x0000,0xFF3F,0x0000,0x007F,0x0000,3989,3990,3989,3990,3990,3991,0,24340,23218,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,23.0,25.1,25.3,-273.2,-273.2,25.1,25.3,25.1,22810,4089,22857,4201,2698,22810,4089,47,112,22857,4201,25.0,25.0,1000,1000,1000,1000,1000,1000,0,0,0,0,0,0,0,0,0,14,0,0,0,0,0,0,0,16,2496,2480,2480,2480,2464,2464,0,0,0,0,1344,2240,1728,1488,1000,1920,0,3188,3197,3196,3179,3176,3204,4400,0,0,0,0,0,0,0,0,0,0.57,11291,2496,2480,2480,2480,2464,2464,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,2704,5877,1457,SUCCESS
    19,2023-07-25 10:42:50,77.724,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,3203,ERROR : Please check C:\Users\Paul\Downloads\BMS-short-test.log.err
    20,2023-07-25 10:42:59,86.613,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,3364,ERROR : Please check C:\Users\Paul\Downloads\BMS-short-test.log.err
    21,2023-07-25 10:43:08,95.697,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,3562,ERROR : Please check C:\Users\Paul\Downloads\BMS-short-test.log.err
    22,2023-07-25 10:43:17,104.950,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,3654,ERROR : Please check C:\Users\Paul\Downloads\BMS-short-test.log.err
    23,2023-07-25 10:43:27,114.234,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,3676,ERROR : Please check C:\Users\Paul\Downloads\BMS-short-test.log.err
    24,2023-07-25 10:43:36,123.562,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,0,0,0,0,0,0,0,0,23.2,25.3,25.5,-273.2,-273.2,19.8,-273.2,-273.2,0,0,0,0,0,,,,,,,-273.2,25.3,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,14,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,3188,3197,3196,3179,3176,3204,4400,0,0,0,0,0,0,0,0,0,0.57,11291,0,0,0,0,0,2416,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,2052,ERROR : Please check C:\Users\Paul\Downloads\BMS-short-test.log.err
    25,2023-07-25 10:43:39,126.716,0x6101,1000,10,0x6081,0,0,65535,1,25.3,23944,0,0,1,100,662,22816,22850,65535,65535,65535,0,0,0x48C0,3,0,0,0,0,0,0x6101,0x0000,0x10,0x0004,0x50,0x0814,0x01B8,0x0000,0x0000,0x0000,0x0000,0xFF3F,0x0000,0x007F,0x0000,3991,3991,3990,3991,3990,3991,0,24342,525,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,23.5,25.3,25.6,-273.2,-273.2,25.3,25.6,25.3,22816,4082,22850,4163,2704,22816,4082,34,81,22850,4163,25.3,25.3,1000,1000,1000,1000,1000,1000,0,0,0,0,0,0,0,0,0,14,0,0,0,0,0,0,0,0,2448,2432,2432,2448,2432,2416,0,0,0,0,1344,2256,1728,1488,1004,1936,0,3188,3197,3196,3179,3176,3204,4400,0,0,0,0,0,0,0,0,0,0.57,11291,2448,2432,2432,2448,2432,2416,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,2704,5877,1527,SUCCESS
    26,2023-07-25 10:43:41,128.868,0x6101,1000,10,0x6001,0,65535,65535,1,25.3,23939,0,0,1,100,662,22816,22850,65535,65535,65535,30552,25200,0x48C0,3,-1843,-15973,-1024,-6900,78,0x6101,0x0000,0x10,0x0004,0x50,0x0814,0x01B8,0x0000,0x0000,0x0000,0x0000,0xFF3F,0x0000,0x007F,0x0000,3989,3990,3989,3990,3991,3991,0,24337,9,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,23.2,25.3,25.6,-273.2,-273.2,25.3,25.6,25.3,22816,4082,22850,4163,2704,22816,4082,34,81,22850,4163,25.3,25.3,1000,1000,1000,1000,1000,1000,0,0,0,0,0,0,0,0,0,14,0,0,0,0,0,0,0,3,2448,2432,2432,2448,2432,2416,0,0,0,0,1344,2256,1728,1488,1004,1936,0,3188,3197,3196,3179,3176,3204,4400,0,0,0,0,0,0,0,0,0,0.57,11291,2448,2432,2432,2448,2432,2416,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,2704,5877,1534,SUCCESS
    27,2023-07-25 10:43:45,132.288,0x0107,1000,10,0x6001,0,65535,65535,1,25.3,23939,0,0,1,100,662,22816,22850,65535,65535,65535,30552,25200,0x48C0,3,-1843,-15973,-1024,-6900,78,0x0107,0x0000,0x10,0x0004,0x50,0x0814,0x01B8,0x0000,0x0000,0x0000,0x0000,0xFF3F,0x0000,0x007F,0x0000,3990,3990,3989,3990,3990,3990,0,24337,23216,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,23.2,25.3,25.6,-273.2,-273.2,25.3,25.6,25.3,22816,4082,22850,4163,2704,22816,4082,34,81,22850,4163,25.3,25.3,1000,1000,1000,1000,1000,1000,0,0,0,0,0,0,0,0,0,14,0,0,0,0,0,0,0,6,2448,2432,2432,2448,2432,2416,0,0,0,0,1344,2256,1728,1488,1004,1936,0,3188,3197,3196,3179,3176,3204,4400,0,0,0,0,0,0,0,0,0,0.57,11291,2448,2432,2432,2448,2432,2416,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,2704,5877,1534,SUCCESS
    28,2023-07-25 10:43:49,136.291,0x0107,1000,10,0x6001,0,65535,65535,1,25.3,23939,0,0,1,100,662,22816,22850,65535,65535,65535,30552,25200,0x48C0,3,-1843,-15973,-1024,-6900,78,0x0107,0x0000,0x10,0x0004,0x50,0x0814,0x01B8,0x0000,0x0000,0x0000,0x0000,0xFF3F,0x0000,0x007F,0x0000,3989,3989,3990,3990,3990,3991,0,24337,23216,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,23.3,25.3,25.6,-273.2,-273.2,25.3,25.6,25.3,22816,4082,22850,4163,2704,22816,4082,34,81,22850,4163,25.3,25.3,1000,1000,1000,1000,1000,1000,0,0,0,0,0,0,0,0,0,14,0,0,0,0,0,0,0,10,2448,2432,2432,2448,2432,2416,0,0,0,0,1344,2256,1728,1488,1004,1936,0,3188,3197,3196,3179,3176,3204,4400,0,0,0,0,0,0,0,0,0,0.57,11291,2448,2432,2432,2448,2432,2416,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,2704,5877,1561,SUCCESS
    29,2023-07-25 10:43:53,140.294,0x0107,1000,10,0x6001,0,65535,65535,1,25.3,23940,0,0,1,100,662,22816,22850,65535,65535,65535,30552,25200,0x48C0,3,-1843,-15973,-1024,-6900,78,0x0107,0x0000,0x10,0x0004,0x50,0x0814,0x01B8,0x0000,0x0000,0x0000,0x0000,0xFF3F,0x0000,0x007F,0x0000,3989,3990,3989,3990,3990,3990,0,24339,23217,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,23.2,25.3,25.6,-273.2,-273.2,25.3,25.6,25.3,22816,4082,22850,4163,2704,22816,4082,34,81,22850,4163,25.3,25.3,1000,1000,1000,1000,1000,1000,0,0,0,0,0,0,0,0,0,14,0,0,0,0,0,0,0,14,2448,2432,2432,2448,2432,2416,0,0,0,0,1344,2256,1728,1488,1004,1936,0,3188,3197,3196,3179,3176,3204,4400,0,0,0,0,0,0,0,0,0,0.57,11291,2448,2432,2432,2448,2432,2416,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,2704,5877,1560,SUCCESS
    30,2023-07-25 10:43:57,144.299,0x0107,1000,10,0x6001,0,65535,65535,1,25.3,23939,0,0,1,100,662,22816,22850,65535,65535,65535,30552,25200,0x48C0,3,-1843,-15973,-1024,-6900,78,0x0107,0x0000,0x10,0x0004,0x50,0x0814,0x01B8,0x0000,0x0000,0x0000,0x0000,0xFF3F,0x0000,0x007F,0x0000,3990,3990,3989,3990,3990,3991,0,24339,23216,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,23.3,25.3,25.6,-273.2,-273.2,25.3,25.6,25.3,22816,4082,22850,4163,2704,22816,4082,34,81,22850,4163,25.3,25.3,1000,1000,1000,1000,1000,1000,0,0,0,0,0,0,0,0,0,14,0,0,0,0,0,0,0,18,2448,2432,2432,2448,2432,2416,0,0,0,0,1344,2256,1728,1488,1004,1936,0,3188,3197,3196,3179,3176,3204,4400,0,0,0,0,0,0,0,0,0,0.57,11291,2448,2432,2432,2448,2432,2416,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,2704,5877,1586,SUCCESS
    31,2023-07-25 10:44:01,148.298,0x0107,1000,10,0x6001,0,65535,65535,1,25.3,23940,0,0,1,100,662,22816,22850,65535,65535,65535,30552,25200,0x48C0,3,-1843,-15973,-1024,-6900,78,0x0107,0x0000,0x10,0x0004,0x50,0x0814,0x01B8,0x0000,0x0000,0x0000,0x0000,0xFF3F,0x0000,0x007F,0x0000,3989,3990,3990,3990,3990,3991,0,24339,23214,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,23.2,25.3,25.6,-273.2,-273.2,25.3,25.6,25.3,22816,4082,22850,4163,2704,22816,4082,34,81,22850,4163,25.3,25.3,1000,1000,1000,1000,1000,1000,0,0,0,0,0,0,0,0,0,14,0,0,0,0,0,0,0,22,2448,2432,2432,2448,2432,2416,0,0,0,0,1344,2256,1728,1488,1004,1936,0,3188,3197,3196,3179,3176,3204,4400,0,0,0,0,0,0,0,0,0,0.57,11291,2448,2432,2432,2448,2432,2416,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,2704,5877,1561,SUCCESS
    32,2023-07-25 10:44:05,152.306,0x0107,1000,10,0x6001,0,65535,65535,1,25.3,23940,0,0,1,100,662,22816,22850,65535,65535,65535,30552,25200,0x48C0,3,-1843,-15973,-1024,-6900,78,0x0107,0x0000,0x10,0x0004,0x50,0x0814,0x01B8,0x0000,0x0000,0x0000,0x0000,0xFF3F,0x0000,0x007F,0x0000,3989,3990,3989,3990,3990,3991,0,24337,23214,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,23.2,25.3,25.5,-273.2,-273.2,25.3,25.5,25.3,22816,4082,22850,4163,2704,22816,4082,34,81,22850,4163,25.3,25.3,1000,1000,1000,1000,1000,1000,0,0,0,0,0,0,0,0,0,14,0,0,0,0,0,0,0,26,2448,2432,2432,2448,2432,2416,0,0,0,0,1344,2256,1728,1488,1004,1936,0,3188,3197,3196,3179,3176,3204,4400,0,0,0,0,0,0,0,0,0,0.57,11291,2448,2432,2432,2448,2432,2416,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,2704,5877,1617,SUCCESS
    33,2023-07-25 10:44:09,156.317,0x0107,1000,10,0x6001,0,65535,65535,1,25.3,23940,0,0,1,100,662,22816,22850,65535,65535,65535,30552,25200,0x48C0,3,-1843,-15973,-1024,-6900,78,0x0107,0x0000,0x10,0x0004,0x50,0x0814,0x01B8,0x0000,0x0000,0x0000,0x0000,0xFF3F,0x0000,0x007F,0x0000,3989,3990,3989,3990,3991,3991,0,24337,23214,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,23.2,25.3,25.5,-273.2,-273.2,25.3,25.5,25.3,22816,4082,22850,4163,2704,22816,4082,34,81,22850,4163,25.3,25.3,1000,1000,1000,1000,1000,1000,0,0,0,0,0,0,0,0,0,14,0,0,0,0,0,0,0,30,2448,2432,2432,2448,2432,2416,0,0,0,0,1344,2256,1728,1488,1004,1936,0,3188,3197,3196,3179,3176,3204,4400,0,0,0,0,0,0,0,0,0,0.57,11291,2448,2432,2432,2448,2432,2416,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,2704,5877,1616,SUCCESS
    34,2023-07-25 10:44:13,160.328,0x0107,1000,10,0x6001,0,65535,65535,1,25.3,23939,0,0,1,100,662,22816,22850,65535,65535,65535,30552,25200,0x48C0,3,-1843,-15973,-1024,-6900,78,0x0107,0x0000,0x10,0x0004,0x50,0x0814,0x01B8,0x0000,0x0000,0x0000,0x0000,0xFF3F,0x0000,0x007F,0x0000,3990,3990,3990,3990,3990,3991,0,24336,23217,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,23.3,25.3,25.5,-273.2,-273.2,25.3,25.5,25.3,22816,4082,22850,4163,2704,22816,4082,34,81,22850,4163,25.3,25.3,1000,1000,1000,1000,1000,1000,0,0,0,0,0,0,0,0,0,14,0,0,0,0,0,0,0,34,2448,2432,2432,2448,2432,2416,0,0,0,0,1344,2256,1728,1488,1004,1936,0,3188,3197,3196,3179,3176,3204,4400,0,0,0,0,0,0,0,0,0,0.57,11291,2448,2432,2432,2448,2432,2416,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,2704,5877,1580,SUCCESS
    35,2023-07-25 10:44:17,164.337,0x0107,1000,10,0x6001,0,65535,65535,1,25.3,23939,0,0,1,100,662,22816,22850,65535,65535,65535,30552,25200,0x48C0,3,-1843,-15973,-1024,-6900,78,0x0107,0x0000,0x10,0x0004,0x50,0x0814,0x01B8,0x0000,0x0000,0x0000,0x0000,0xFF3F,0x0000,0x007F,0x0000,3990,3990,3989,3990,3990,3991,0,24336,23216,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,23.2,25.2,25.5,-273.2,-273.2,25.3,25.5,25.3,22816,4082,22850,4163,2704,22816,4082,34,81,22850,4163,25.3,25.2,1000,1000,1000,1000,1000,1000,0,0,0,0,0,0,0,0,0,14,0,0,0,0,0,0,0,38,2448,2432,2432,2448,2432,2416,0,0,0,0,1344,2256,1728,1488,1004,1936,0,3188,3197,3196,3179,3176,3204,4400,0,0,0,0,0,0,0,0,0,0.57,11291,2448,2432,2432,2448,2432,2416,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,2704,5877,1627,SUCCESS
    36,2023-07-25 10:44:21,168.352,0x0107,1000,10,0x6001,0,65535,65535,1,25.2,23940,0,0,1,100,662,22816,22850,65535,65535,65535,30552,25200,0x48C0,3,-1843,-15973,-1024,-6900,78,0x0107,0x0000,0x10,0x0004,0x50,0x0814,0x01B8,0x0000,0x0000,0x0000,0x0000,0xFF3F,0x0000,0x007F,0x0000,3990,3990,3989,3990,3990,3991,0,24336,23217,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,23.2,25.3,25.5,-273.2,-273.2,25.3,25.5,25.3,22816,4082,22850,4163,2704,22816,4082,34,81,22850,4163,25.3,25.2,1000,1000,1000,1000,1000,1000,0,0,0,0,0,0,0,0,0,14,0,0,0,0,0,0,0,42,2448,2432,2432,2448,2432,2416,0,0,0,0,1344,2256,1728,1488,1004,1936,0,3188,3197,3196,3179,3176,3204,4400,0,0,0,0,0,0,0,0,0,0.57,11291,2448,2432,2432,2448,2432,2416,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,2704,5877,1644,SUCCESS
    37,2023-07-25 10:44:25,172.356,0x0107,1000,10,0x6001,0,65535,65535,1,25.3,23940,0,0,1,100,662,22816,22850,65535,65535,65535,30552,25200,0x48C0,3,-1843,-15973,-1024,-6900,78,0x0107,0x0000,0x10,0x0004,0x50,0x0814,0x01B8,0x0000,0x0000,0x0000,0x0000,0xFF3F,0x0000,0x007F,0x0000,3990,3990,3990,3990,3990,3991,0,24337,23216,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,23.2,25.2,25.5,-273.2,-273.2,25.2,25.5,25.2,22816,4082,22850,4163,2704,22816,4082,34,81,22850,4163,25.3,25.2,1000,1000,1000,1000,1000,1000,0,0,0,0,0,0,0,0,0,14,0,0,0,0,0,0,0,46,2448,2432,2432,2448,2432,2416,0,0,0,0,1344,2256,1728,1488,1004,1936,0,3188,3197,3196,3179,3176,3204,4400,0,0,0,0,0,0,0,0,0,0.57,11291,2448,2432,2432,2448,2432,2416,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,2704,5877,1686,SUCCESS
    38,2023-07-25 10:44:29,176.366,0x0107,1000,10,0x6001,0,65535,65535,1,25.2,23940,0,0,1,100,662,22816,22850,65535,65535,65535,30552,25200,0x48C0,3,-1843,-15974,-1024,-6900,78,0x0107,0x0000,0x10,0x0004,0x50,0x0814,0x01B8,0x0000,0x0000,0x0000,0x0000,0xFF3F,0x0000,0x007F,0x0000,3990,3990,3990,3990,3991,3991,0,24336,23217,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,23.2,25.2,25.5,-273.2,-273.2,25.2,25.5,25.2,22816,4082,22850,4163,2704,22816,4082,34,81,22850,4163,25.3,25.2,1000,1000,1000,1000,1000,1000,0,0,0,0,0,0,0,0,0,14,0,0,0,0,0,0,0,50,2448,2432,2432,2448,2432,2416,0,0,0,0,1344,2256,1728,1488,1004,1936,0,3188,3197,3196,3179,3176,3204,4400,0,0,0,0,0,0,0,0,0,0.57,11291,2448,2432,2432,2448,2432,2416,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,2704,5877,1720,SUCCESS
    39,2023-07-25 10:44:33,180.373,0x0107,1000,10,0x6001,0,65535,65535,1,25.2,23940,0,0,1,100,662,22816,22850,65535,65535,65535,30552,25200,0x48C0,3,-1843,-15974,-1024,-6900,78,0x0107,0x0000,0x10,0x0004,0x50,0x0814,0x01B8,0x0000,0x0000,0x0000,0x0000,0xFF3F,0x0000,0x007F,0x0000,3990,3990,3989,3990,3991,3991,0,24336,23217,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,23.2,25.2,25.5,-273.2,-273.2,25.2,25.5,25.2,22816,4082,22850,4163,2704,22816,4082,34,81,22850,4163,25.3,25.2,1000,1000,1000,1000,1000,1000,,0,0,0,0,0,0,,,,,,,,0,0,,,,,,,2432,2416,,,,,,,,,1004,1936,,,,,,3176,3204,,,,,,0,0,,,,,,,,,,2432,2416,,,,,,,,,,,,,,,,,,,2616,ERROR : Please check C:\Users\Paul\Downloads\BMS-short-test.log.err
    40,2023-07-25 10:44:38,185.927,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,3884,ERROR : Please check C:\Users\Paul\Downloads\BMS-short-test.log.err
    41,2023-07-25 10:44:48,195.495,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,3862,ERROR : Please check C:\Users\Paul\Downloads\BMS-short-test.log.err
    42,2023-07-25 10:44:57,205.078,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,3877,ERROR : Please check C:\Users\Paul\Downloads\BMS-short-test.log.err
    43,2023-07-25 10:45:07,214.694,0x6101,1000,10,0x6081,0,0,0,0,25.5,23943,0,0,100,0,0,0,3450,0,0,0,0,0,0x0040,3,0,0,0,0,0,0x6101,0x0100,0x10,0x0004,0x50,0x0814,0x01B8,0x0000,0x0000,0x0000,0x0000,0xFF3F,0x0000,0x007F,0x0000,3990,3990,3990,3991,3991,3991,0,24341,8336,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,23.7,25.5,25.8,-273.2,-273.2,25.5,25.8,25.5,0,0,0,0,0,0,0,34,81,0,0,25.5,25.5,1000,1000,1000,1000,1000,1000,0,0,0,0,0,0,0,0,0,14,0,0,0,0,0,0,0,0,2448,2448,2448,2432,2432,2432,0,0,0,0,1352,2272,1728,1488,1008,1936,0,3188,3197,3196,3179,3176,3204,4400,0,0,0,0,0,0,0,0,0,0.57,11291,2448,2448,2448,2432,2432,2432,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,1675,SUCCESS
    44,2023-07-25 10:45:10,217.509,0x6101,1000,10,0x6001,0,65535,65535,1,25.5,23939,0,0,1,100,662,22813,22847,65535,65535,65535,30552,25200,0x48C0,3,-1843,-15969,-1024,-6900,78,0x6101,0x0000,0x10,0x0004,0x50,0x0814,0x01B8,0x0000,0x0000,0x0000,0x0000,0xFF3F,0x0000,0x007F,0x0000,3989,3990,3989,3989,3990,3991,0,24337,12,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,23.4,25.5,25.8,-273.2,-273.2,25.5,25.8,25.5,22813,4104,22847,4185,2705,22813,4104,34,81,22847,4185,25.5,25.5,1000,1000,1000,1000,1000,1000,0,0,0,0,0,0,0,0,0,14,0,0,0,0,0,0,0,2,2448,2448,2448,2432,2432,2432,0,0,0,0,1352,2272,1728,1488,1008,1936,0,3188,3197,3196,3179,3176,3204,4400,0,0,0,0,0,0,0,0,0,0.57,11291,2448,2448,2448,2432,2432,2432,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,2704,5877,1705,SUCCESS
    45,2023-07-25 10:45:13,220.463,0x0107,1000,10,0x6001,0,65535,65535,1,25.5,23938,0,0,1,100,662,22813,22847,65535,65535,65535,30552,25200,0x48C0,3,-1843,-15969,-1024,-6900,78,0x0107,0x0000,0x10,0x0004,0x50,0x0814,0x01B8,0x0000,0x0000,0x0000,0x0000,0xFF3F,0x0000,0x007F,0x0000,3989,3989,3989,3990,3990,3991,0,24337,23217,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,23.4,25.5,25.8,-273.2,-273.2,25.5,25.9,25.5,22813,4104,22847,4185,2705,22813,4104,34,81,22847,4185,25.5,25.5,1000,1000,1000,1000,1000,1000,0,0,0,0,0,0,0,0,0,14,0,0,0,0,0,0,0,5,2448,2448,2448,2432,2432,2432,0,0,0,0,1352,2272,1728,1488,1008,1936,0,3188,3197,3196,3179,3176,3204,4400,0,0,0,0,0,0,0,0,0,0.57,11291,2448,2448,2448,2432,2432,2432,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,2704,5877,1720,SUCCESS
    46,2023-07-25 10:45:17,224.472,0x0107,1000,10,0x6001,0,65535,65535,1,25.5,23938,0,0,1,100,662,22813,22847,65535,65535,65535,30552,25200,0x48C0,3,-1843,-15969,-1024,-6900,78,0x0107,0x0000,0x10,0x0004,0x50,0x0814,0x01B8,0x0000,0x0000,0x0000,0x0000,0xFF3F,0x0000,0x007F,0x0000,3989,3990,3989,3990,3990,3991,0,24337,23214,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,23.5,25.5,25.9,-273.2,-273.2,25.5,25.9,25.5,22813,4104,22847,4185,2705,22813,4104,34,81,22847,4185,25.5,25.5,1000,1000,1000,1000,1000,1000,0,0,0,0,0,0,0,0,0,14,0,0,0,0,0,0,0,9,2448,2448,2448,2432,2432,2432,0,0,0,0,1352,2272,1728,1488,1008,1936,0,3188,3197,3196,3179,3176,3204,4400,0,0,0,0,0,0,0,0,0,0.57,11291,2448,2448,2448,2432,2432,2432,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,2704,5877,1790,SUCCESS
    47,2023-07-25 10:45:21,228.486,0x0107,1000,10,0x6001,0,65535,65535,1,25.5,23938,0,0,1,100,662,22813,22847,65535,65535,65535,30552,25200,0x48C0,3,-1843,-15969,-1024,-6900,78,0x0107,0x0000,0x10,0x0004,0x50,0x0814,0x01B8,0x0000,0x0000,0x0000,0x0000,0xFF3F,0x0000,0x007F,0x0000,3989,3990,3989,3990,3990,3991,0,24336,23216,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,23.5,25.5,25.8,-273.2,-273.2,25.5,25.8,25.5,22813,4104,22847,4185,2705,22813,4104,34,81,22847,4185,25.5,25.5,1000,1000,1000,1000,1000,1000,0,0,0,0,0,0,0,0,0,14,0,0,0,0,0,0,0,13,2448,2448,2448,2432,2432,2432,0,0,0,0,1352,2272,1728,1488,1008,1936,0,3188,3197,3196,3179,3176,3204,4400,0,0,0,0,0,0,0,0,0,0.57,11291,2448,2448,2448,2432,2432,2432,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,2704,5877,1797,SUCCESS
    48,2023-07-25 10:45:25,232.487,0x0107,1000,10,0x6001,0,65535,65535,1,25.5,23938,0,0,1,100,662,22813,22847,65535,65535,65535,30552,25200,0x48C0,3,-1843,-15969,-1024,-6900,78,0x0107,0x0000,0x10,0x0004,0x50,0x0814,0x01B8,0x0000,0x0000,0x0000,0x0000,0xFF3F,0x0000,0x007F,0x0000,3989,3990,3989,3990,3990,3991,0,24337,23214,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,23.4,25.5,25.8,-273.2,-273.2,25.5,25.8,25.5,22813,4104,22847,4185,2705,22813,4104,34,81,22847,4185,25.5,25.5,1000,1000,1000,1000,1000,1000,0,0,0,0,0,0,0,0,0,14,0,0,0,0,0,0,0,17,2448,2448,2448,2432,2432,2432,0,0,0,0,1352,2272,1728,1488,1008,1936,0,3188,3197,3196,3179,3176,3204,4400,0,0,0,0,0,0,0,0,0,0.57,11291,2448,2448,2448,2432,2432,2432,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,2704,5877,1750,SUCCESS
    49,2023-07-25 10:45:29,236.491,0x0107,1000,10,0x6001,0,65535,65535,1,25.5,23938,0,0,1,100,662,22813,22847,65535,65535,65535,30552,25200,0x48C0,3,-1843,-15969,-1024,-6900,78,0x0107,0x0000,0x10,0x0004,0x50,0x0814,0x01B8,0x0000,0x0000,0x0000,0x0000,0xFF3F,0x0000,0x007F,0x0000,3989,3989,3989,3990,3990,3991,0,24337,23216,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,23.5,25.5,25.8,-273.2,-273.2,25.5,25.8,25.5,22813,4104,22847,4185,2705,22813,4104,34,81,22847,4185,25.5,25.5,1000,1000,1000,1000,1000,1000,0,0,0,0,0,0,0,0,0,14,0,0,0,0,0,0,0,21,2448,2448,2448,2432,2432,2432,0,0,0,0,1352,2272,1728,1488,1008,1936,0,3188,3197,3196,3179,3176,3204,4400,0,0,0,0,0,0,0,0,0,0.57,11291,2448,2448,2448,2432,2432,2432,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,2704,5877,1785,SUCCESS
    50,2023-07-25 10:45:33,240.505,0x0107,1000,10,0x6001,0,65535,65535,1,25.5,23939,0,0,1,100,662,22813,22847,65535,65535,65535,30552,25200,0x48C0,3,-1843,-15969,-1024,-6900,78,0x0107,0x0000,0x10,0x0004,0x50,0x0814,0x01B8,0x0000,0x0000,0x0000,0x0000,0xFF3F,0x0000,0x007F,0x0000,3990,3990,3989,3989,3990,3991,0,24337,23214,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,23.4,25.5,25.8,-273.2,-273.2,25.5,25.8,25.5,22813,4104,22847,4185,2705,22813,4104,34,81,22847,4185,25.5,25.5,1000,1000,1000,1000,1000,1000,0,0,0,0,0,0,0,0,0,14,0,0,0,0,0,0,0,25,2448,2448,2448,2432,2432,2432,0,0,0,0,1352,2272,1728,1488,1008,1936,0,3188,3197,3196,3179,3176,3204,4400,0,0,0,0,0,0,0,0,0,0.57,11291,2448,2448,2448,2432,2432,2432,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,2704,5877,1758,SUCCESS
    
    AURA-7-25-config.gg.csv

  • Hello Hrishikesh,

    The only way to reduce the current for the protection is using a larger sense resistor since all the hardware overcurrent protections are based on voltages across the sense resistor. there is not another way to lower the absolute minimum threshold.

    The log seems to cut out at each protection, I'm not sure why this is occurring. It looks like you have multiple PF alerts triggered, something seems wrong with the setup since the log should continue as long as the gauge has power.

    Sincerely,

    Wyatt Keller