This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ34Z100: LTO battery cells chemistry

Part Number: BQ34Z100

Hello,

We have developed an electronic module using the BQ34z100 gauge circuit with LTO cells. I need to find out the chemistryID or other parameters required for accurate battery state measurement.

The schematics of open-source module SOLARMINIBAT01 is available here, in the repository.

We tried to obtain the chemistryID based on the online estimator from measurements taken with the TI battery gauge programmer. However, we received an empty report from the online estimator, and it couldn't determine the chemistryID from our measurements.

Fullscreen
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
0 0 0
0 0 0
0 0 0
0 0 0
0 0 0
0 0 0
0 0 0
0 0 0
0 0 0
0 0 0
0 0 0
0 0 0
0
Summary of all IDs with max. DOD deviation below 3%
Chem ID max DOD error, % Max R deviation, ratio
0 0 0
Warning: Deviation is above recommended level. New chem ID needs to be released for this cell. Please contact your TI representative to send the cell to Dallas for characterization
XXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXX

Is it possible to determine the chemistryID based on, for example, the datasheet or some detailed cell parameters?

We have used this batteries: https://files.gwl.eu/inc/_doc/attach/StoItem/7015/GWL_LTO1865_Rechargeable.pdf

Thank you.