This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi team,
Can the input and charging current sense resistor RAC and RSR be 5-mΩ when the input and charging currents are both bigger than 8.2A?
Best Regards
Silvia Gao
Hello Silvia,
There should not be an issue using a 5-mΩ current sense resistor for the BQ24780s, The BQ24780s is designed to use a default sense resistor of 10-mΩ, with this sense resistor value the BQ24780s can provide a maximum charge current of 8.128A. There should not be an issue using a 5-mΩ current sense resistor, however it might be better to choose a battery charger that is reccommneded for higher charging current: Battery Charger
Best Regards,
Christian.
Hi Christian,
The customer plans to use 5-mΩ resistor as both charge and input current sense resistor, and he has several questions as below:
1. For PMON Gain, what does 0 and 1 represent respectively when RAC = RSR = 5-mΩ? Does 0 represent 0.125uA/W and 1 represent 0.5uA/W?
2. To support hybrid power boost mode, what is the minimum input current need to be set to when RAC = RSR = 5-mΩ? 1536mA*0.5?
3.How to set charge current register (REG0x14) and input current register (REG0x3F) when RAC = RSR = 5-mΩ? Set value = Target value*0.5?
4. In the formula that calculates IPMON below, is IBAT and IIN respectively equal to the read back value of register * 2 when RAC = RSR = 5-mΩ?
5. What will happen if an unreasonable Gain setting causes IPMON exceeding the maximum value in the table? Will IPMON still keep 160uA and the device display an error of 160uA?
Thanks for your answer!
Best Regards
Silvia Gao
Hello Silvia,
For PMON Gain, what does 0 and 1 represent respectively when RAC = RSR = 5-mΩ? Does 0 represent 0.125uA/W and 1 represent 0.5uA/W?
Yes.
2. To support hybrid power boost mode, what is the minimum input current need to be set to when RAC = RSR = 5-mΩ? 1536mA*0.5?
3,072mA it would be double the value if you switched from RAC = RSR = 10-mΩ to RAC = RSR = 5-mΩ.
3.How to set charge current register (REG0x14) and input current register (REG0x3F) when RAC = RSR = 5-mΩ? Set value = Target value*0.5?
It would be double the value if you switched from RAC = RSR = 10-mΩ to RAC = RSR = 5-mΩ.
In the formula that calculates IPMON below, is IBAT and IIN respectively equal to the read back value of register * 2 when RAC = RSR = 5-mΩ?
Yes
What will happen if an unreasonable Gain setting causes IPMON exceeding the maximum value in the table? Will IPMON still keep 160uA and the device display an error of 160uA?
The BQ24780s is designed to use a default sense resistor of 10-mΩ, We do not have data to provide this information.
Best Regards,
Christian.