Hi,
I work recently on bq78pl116, to update our BMS running for about a year on bq78pl114.
Bq detects when the HSC or HOCD, he do not want to clear the flag.
When there is no detection, the circuit works properly !
We see the recovery, but the flag does not turn off and therefore the MOSFETs are set to OFF.
A single error is visible in history.
To clear the flag, I am obliged to make a reset.(Safe disconnect and reconnect)
The same problem is present on EVM.
Change parameters for HSC or Hocdé do not change.
Is it a bug?
Can anyone help me?
Use :
Bqwizard 3.1.0
Firmware FW_0002_0000_6000_0719.enc
BQ78pl116EVM and various BMS of our manufacturing