Following is the requirement in my application:
- Input Voltage: 2.3V to 4.1V
- Output Voltage: 5.5V
- Maximum Output Current (Maximum Load Current): 0.6A
When ripple percentage is considered around 40 percent of Input current, the ripple current will not fall in the recommended range (0.8A to 2A) for certain load currents. How to size the inductor in such a scenario?