This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28070: Could we use UCC28070 Implement interleave DC-DC buck

Part Number: UCC28070
Other Parts Discussed in Thread: UCC28220

Dear Expert

Could we use UCC28070   Implement interleave DC-DC buck .Or some other way to implemet DC-DC interleave buck .

Our input is 220V DC ,and output is 120V ,100A DC .

  • Hi Gabriel,

    Thank you for the query on UCC28070.

    To be honest, UCC28070 has not been tried and tested in the DC buck configuration. One of the concerns is if the current synthesizer can still work ok if using the device in buck PFC. The down-slope of current is calculated/estimated inside of the IC with the intended use with boost concerter.

    You can check with UCC28220 for this application.

    Regards,

    Harish