Other Parts Discussed in Thread: PMP40261
Dear Expert
1. The chip does not have AC undervoltage protection. After turning off AC, because the VCC of the chip is powered by an external auxiliary source, the chip will be fully driven after AC is turned off, making it impossible to achieve AC fast switching on and off. Therefore, an AC undervoltage circuit needs to be added to the periphery of the circuit;
2. When switching the output power of PFC from 0W to 800W, the PFC current will reach the maximum current value of OCP at the moment of switching, and the chip will turn off the PFC drive, resulting in an abnormal current waveform;
3. Is it normal for two different types of drives to occur when the output is unloaded and lightly loaded (0-60W), with one having more drives and the other not being driven at all? What modifications are needed to make the two drives consistent;
4. VCCP compensates for current sampling through R5, and what is the purpose of this compensation;