Other Parts Discussed in Thread: BQ25730, BQ25731, , PMP41013, TPS56339, BQ25792
Hello,
I want to develop an application using the TPS25750 and the BQ25730. I am fully aware that the official compatibility is only with BQ25731 so I tried using the customization app with that setting and see what I get out.
Unfortunately when I select the BQ25731, I cannot select a lower voltage for the battery charging than 9.2V, but the charger is compatible with 1S cells, so I expect I could select 4.2V as the charging voltage. Am I missing something?
Regarding compatibility with the BQ25730:
Is the TPS25750 ever checking the charger ID too? Both chargers have the same I2C slave address, but different charger IDs.
Package/pin wise, the BQ25730 and BQ25731 are identical with the only difference being that the BQ25730 has power path and a pin to drive the power path FET. They have the same package and pinout where the mosfet driver pin is just NC on the BQ25731. Could I assume that if one would not care about the power path functionality, the BQ25730/1 are fully interchangeable?
The registers appear to be such constructed that what is implemented on the BQ25730 for power path, is reserved on the BQ25731, so software developed for the non power path BQ25731 version will work exactly the same on the power path version BQ25730, with default power path parameters (as a matter of fact it seems that the RESERVED bits in all the BQ25731's registers have the values such that they correspond to the default values in the BQ25730). This was done by side-by-side comparing the two datasheets register mapping and register descriptions. Am I correct in my assumption that software written for BQ25731 is directly compatible with BQ25730?
Thank you and Best Regards,
Filip-Razvan Lupas.