This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
The datasheet of the TPS61288 recommends up to 4.7uH, but the Web Bench suggests going to 10uH. Is it a problem going to 10uH?
Hi Ahmad,
The two of inductance are theoretically all ok. Usually, we prefer a ripple ratio of 20% to 40% to optimize the inductor.
Webench is a reference design but not the optimized design.
A large inductance is hard to choose and not necessary.
In your application, choosing 2.2uH or 3.3uH is enough.
Please refer to the calculation tool of the device.
6646.TPS61288 Calculation tool.xlsx
Best Regards
Fergus