Other Parts Discussed in Thread: UNIFLASH, TM4C123GH6PM, TPS25750
Hi,
Can I receive the TIVA firmware shipped with the TPS25750EVM?
Thanks,
Nate
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Can I receive the TIVA firmware shipped with the TPS25750EVM?
Thanks,
Nate
Hello Nate,
We do not provide the firmware for the EVM.
Based upon the previous thread, I do no believe we can support this request. You do have the option of using a tool like Uniflash to read out the binary image from the TM4C123 but I do not believe this would be very beneficial.
If you going to use an MCU like the TM4C123GH6PM, then I would recommend starting with the examples provided: https://www.ti.com/tool/SW-TM4C
<TivaWare_Installation>\examples\peripherals\i2c
Regards,
Chris
So if I did buy the TPS25750EVM and managed to brick the onboard TIVA chip, TI wouldnt provide the firmware to re-flash it? I don't need/want the source code, just a binary that I can flash using a launchpad or something.
All I want to have is a way to flash TI's TPS25750 chip in my custom design with TI's already provided flash generation software...
Nate