Hello,
I am wanting to setup a simple COM to I2C microcontroller to properly interface with the TPS25750 Application Customization Tool's COM interface. The intent being streamlining the flashing process for new TPS25750 configurations.
At the moment, I can see that the application customization tool "pings" the selected COM port with "i2ce 2 400 80 64 0 0". I can make some assumptions on what it is trying to do, but have no idea what it wants as a response.
Can someone point me to where I might find this documentation?
This would greatly speed my development process with this chip.
Thanks,
Nate