This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM2595: alternative

Part Number: LM2595

Hello,

Can you please explain me what are the main differences between de following Power Conventors:

LM2595SX-ADJ/NOPB and LM2595SX-5.0/NOPB

Regards,

Kathleen

  • Hi Eddy,

    Thank you for considering our products.  The major difference can be easily seen in the block diagram:  the FB resistors are internal for 5V version, and external for ADJ.  You save two resistors.  You can also use ADJ version to produce 5Vout but you need two external resistors.  Other than these, the two devices are the same.

    Hope this clarifies.

    Best Regards,

    Youhao