This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM25149: LM25149

Part Number: LM25149


Hi Sir,

I use LM25149 to design a power Vin=24Vdc, Vout=18V@15A, I design a circuitry similar EVM board, I remove R6 between AEFVDDA and Vcc, VCCx is connected GND, when I power input 24Vdc for 10 seconds, the power supply overload, I found an issue AEDVDDA  is short to GND after I power off and checking, do you have any ideas about my power design?   

Note: power components

1. NMOS FET: IAUC60N04S6L039

2. Inductor: 0.1uH/32.5A  (L 0.1uH/32.5A 20% IHLP2525CZERR10M01)

3. Circuitry is the same EVM, I remove R6 between AEFVDDA and Vcc

4. VCCx = GND

John Chang

2023/9/6