This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPSM41625: TPSM41625 ILIM

Part Number: TPSM41625


For the ILIM-Function of TPSM41625:

Is RILIM specified for the (5) values in Table 7-12 only - or is any value in between (i.e. 47K) also possible?

Thanks!

Olaf

  • Hi Olaf,

    The datasheet doesn't specify being able to use values in between, I believe this device uses some type of pin strapping to select the settings. Which means you need to use the same nominal resistance value in the table, and not values in between.

    Thanks,

    Joseph