Part Number: BQ2026EVM
Hi,
This mail is regarding BQ2026 IC of TI. Request you to address the below queries.
1) BQ2026EVM, what are the components this Kit contains? Does it include Reva board along with EV2300 HPA002 interface board ?
2) If it doesn’t contain EV2300 HPA002 interface board, can we any other Microcontroller or use personal laptop to program the BQ2026 reva board ? Please do mention if there are any specific microcontrollers that can be used.
3) Is Possible to read the data written in BQ2026 using any CPU? Or is there a specific host that has to be used to read the data?
4) Can multiple BQ2026 be connected to single SDQ bus and read data one after the other just like how One wire protocol function?
5) Its mentioned that BQ2026 is OTP device, does that mean it can be overwritten after initial programming?