This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5157-Q1: LM5157-Q1 can not provide enough current

Part Number: LM5157-Q1


Hey all,

I have fabricated a PCB with the LM5157-Q1 see the attached schematic. This schematic was review and blessed by TI in another thread. It is working fine at a 2.841A load but when increased to a 3.055A load the regulator can not keep up, see attached screen shot. Anything I can do to be stable at a higher load?

Sincerely,

Corey