Hi Team,
As title, does the chip can support two 50% PWM signal (+/-180 degree) with manual dead time control?
For example.
Regards,
Roy
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Roy,
Absolutely. This devices is designed to provide complementary signal (180 degrees shifted) with a max duty cycle of 50% each and with a programmable dead time. To program switching frequency and dead time, use pin CT and DIS. Please refer to pg. 5 and pg. 6 to design those parameters.
If you have any further questions, let me know replying to this thread.
Hi Manuel,
I don't clearly understand the calculation of the clk for the part.
If we need 60Hz PWM signal(+/-180degree) with 3% dead time. How can we design CT and DIS pin R/C?
Regards,
Roy
Hi Roy,
Use 1st order equations showed in pg. 7. Some considerations:
-Tdischarge is the dead time between driver signals (OUTA and OUTB).
-Oscillator frequency fosc is twice switching frequency fs.
Parameters:
fs=60Hz; fosc=120Hz; Tdischarge=(0.03)*(1/120Hz)
Equations:
1.36*Rb*Ct=Tdischarge
5.9/[(Ra+8*Rb)*Ct]=fosc
You can start setting Ra value and then calculate Rb and Ct values. One example for your case:
Ct=200pF; Rb=920ohm; Ra=238.5Kohm
Please, take into consideration that these values are within the range of +/-20% of the real values. Measuring the charge and discharge time at the SYNC pin is recommended to verify them.
If you have any further questions, let me know replying to this thread.