This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC2801-EP: UCC2801-EP

Part Number: UCC2801-EP

Hello, 

I am using the UCC2801QDREP for one of my designs and I want to change it by the UCC2801MDREP. The only difference seen between the two versions is the temperaure range, -40 to 125°C for UCC2801QDREP  and -55 to 125°C for UCC2801MDREP.

I would like to know :

  1. Except for the temperature holding, what do we get for the UCC2801MDREP compared to the UCC2801QDREP version ? 
  2. Has the UCC2801MDREP version been specifically tested?
  3. As for the UCC2801MDREP version, I would like to know if the UCC2801QDREP has been qualified at -55°C to 125°C.

The aim is to identify differences between the UCC2801QDREP  and UCC2801MDREP.

Thank you for your support.

Best regards. 

Moha