Other Parts Discussed in Thread: BQ40Z50
Customerm is using BOTHOFF functionality on the DFETOFF pin in order to disable power on the battery connector when the battery is unplugged from the device. But BQ76942 doesn't enter sleep mode when unplugging the battery.
Reading in the manual it seems a microcontroller is needed for that? That is not an option due to no uC being available.
Do you have any idea for that?
They thought about introducing a "fake failure" which would trigger the logic to turnoff the FETS? For example they could use a second thermistor input and design a small circuit that gives a pulse upon disconnection that gets interpreted as FET under temperature and triggers the protection.
Any other/better idea?