Other Parts Discussed in Thread: BQSTUDIO,
Hi Ti Experts,
we want to use the bq76952 in standalone mode for a 16S6P (21,6Ah) LiFePo application.
So far we have designed and produced a first PCB version.
We are using the BOTHOFF functionality to switch off the FETs if the battery is not mounted in the system.
That is working so for.
Also I want that the bq enters the SLEEP-Mode. For that I have activated the SLEEP-Bit:
If the battery is mounted in the system and the BOTHOFF-Pin (Pin30) ist conntected to Battery-Minus the bq enters the SLEEP-Mode:
If the battery is not in the system (BOTHOFF-Pin is connetect to 3V3) the bq stays in NORMAL-Mode:
Is there any opportunity to enter SLEEP-MODE if the battery is not mounted in the system (BOTHOFF-Pin is connetect to 3V3)?
Thanks for helping us.
Klaus