This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5160-Q1: LM5160-Q1 question

Part Number: LM5160-Q1
Other Parts Discussed in Thread: LM5160

Hello

i have designed a DC-DC converter  and just want to make sure that i have calculated all values right, attached is the schematic for your reference...

input : 19-65V

output: 15V - 2A

Frequency : 500Khz

Soft start : 20ms

1) is it safe to use a larger then 100nF CSS capacitor for the soft start, and if yes how large is ?

2) not fully understood the frequency limitation from the datasheet, am i ok with the 500Khz ?

3) calculated resistors or any other remarks ?

LM5160-Q1 sch.pdf

thanks in advance