Part Number: TPS563200
Hi Team,
Reference to the previous discussions, https://e2e.ti.com/support/power-management-group/power-management/f/power-management-forum/1267943/tps563200-ic-gets-damaged-for-minimum-load-of-500ma/4803686#4803686 we had rerouted the PCB and the design worked for around 100 hours.
Testing: Input 12V2A, Output 5V3A. Tested for 100 Hours.
Input: Lab Power Source, Output: Lab DC Load
The design from the TI webench was for an input range for 11.5V to 12.5V.
When the input voltage falls below 11.5V, the Low Side FET gets shorted. Falls below meaning, the Low Side FET gets shorted when the input voltage is for example, 11.45V (or lower).
We went back the WeBench and tried to adjust the range to 11.0V to 12.5V. For this change, there was no change with respect to the components.
Question #1: How do we make sure the TPS563200 can operate in a wider input range (for example, 10.5V to 12.5V).
Question #2: Any possibility of disabling the TPS563200 functionality when the input voltage range is outside the 'design range'. We did explore the EN pin, but want the suggestion from the experts on the best way to handle the above range (10.5V to 12.5V) without damaging the TPS563200 module.
Regards,
Sadashivan