This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ77915: Enquiry about Choosing Current Sense Resistor Value

Part Number: BQ77915

According to datasheet page 39 picture shown,

Although page 41 has some explanation about it, but still lack of understanding to choose suitable value for current sense resistor.

Assume using 5 series 5Ah battery, with 1C-rate (5 A) charge and 3C-rate (15 A) discharge and allow maximum load of 40A, 800W. So can u suggest a suitable value and provide the datasheet of current sense?. Please provide some explanation also or calculation method.

Thank you very much:)