This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM3880: LM3880 for power sequencing of Zynq Ultrascale

Part Number: LM3880
Other Parts Discussed in Thread: TIDA-01480, , TPS568215, TPS56C215

I am designing a custom board using Zynq Ultrascale and I am using TIDA-01480 power supply design. I am planning to use LM3880 for power sequencing.

I am confused with EN pin of LM3880. In TIDA-01480, the first priority buck converter is TPS568215 and TPS56C215. i have the following questions:

1) Can I give the VIN(5V) to the enable pin of the above buck converters?

2)If so, Is it OK to give the PGOOD signal from any of these buck converters to the enable pin of LM3880? Please find the attachment.

3) If this method is not possible, how can I implement power sequencing using TIDA-01480 and LM3880 for Zynq Ultrascale.

Thank you in advance