Part Number: LM5155
Other Parts Discussed in Thread: LM5157, , LM5156
Hello TI Engineers,
Currently the LM5155, LM5156 as well as the LM5157/5158 SEPIC EVMs use coupled inductors in the layout. Based on the TI article "Benefits of a coupled-inductor SEPIC converter", the SEPIC can be designed with
2 individual non-coupled inductors. Does TI have a guide on how to layout the LM5155/6/7/8 SEPIC using 2 individual inductors? Can we follow the LM5155/6/7/8 SEPIC EVM and replace the L1 footprint with the 2 individual inductors next to each other in the same area as the current L1 coupled inductors.
Another question: What are the other parameters for the selecting the MOSFET for the LM5155 SEPIC design?
The current MOSFET in the LM5155 SEPIC EVM is ON Semiconductor NVMFS5C645NLWFAFT1G
If we were to find an alternate part to use, what are the most important parameters to match?
Thanks,
Deniel