Other Parts Discussed in Thread: TPS65987, TVS2200
Hi
Could you help check the TUSB544 schematic and any need to adjust ,Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Please double check and make sure the ESD component ICMEF052P120MFR is appropriate. Otherwise TUSB544 portion of the schematic looks ok.
I will ask the PD team to check on the TPS65987.
Thanks
David
Hello,
I will give feedback by Friday. May I get some background on the application of this design?
Thanks,
Chris
C266 - Change to 4.7uF capacitor
C273/C274 - We recommend 10uF. Remove one of these
C267-C272 - We recommend 47uF (max 120uF) for Source, 10uF for Sink
VBUS1/VBUS2 - Add a TVS2200 or Schottkey diode close to pin
I2C1 SCL/SDA look to be pulled up to 1.8V via 1P8S and LDO_3V3. Please check. Should be pulled up to 3.3V from LDO_3V3
Ground GPIOs that are unused (GPIO16/GPIO17)
It still has to be Pull-up to LDO_3V3 and then converted to 1.8V and connected to the SOC
This would be recommended way to do it.
Another way to do this is to take the LDO_3V3 and use an LDO to convert to 1.8V. Then you can have the TPS65987 I2C lines connected to 1.8V pull-ups. This would also require a configuration change in the TPS65987 though.
The main goal is to always be sure the I2C lines coming from/to the PD are powered by LDO_3V3 to avoid any conditions where the PD cannot communicate to other devices.