Other Parts Discussed in Thread: UCC28250
Hello,
I have configured the external circuit of controller to get the 90KHz at 45% duty PWM on primary outputs. Hence the RT ~82Kohm and external PWM applied across this resistor.
Test Condition#1: Running with circuit config: 90KHz and 45% duty.
Controller runs as expected at 90KHz and 45% duty cycle.
Test Condition#2: While running as above, external sync pwm (220KHz @ 50% duty cycle) is applied across RT resistor.
Controller gives the 110KHz PWM at output with 49% duty cycle.

Test Condition #3: But as soon as you remove the sync PWM, controller is not going going back to PWM frequency set by resistor RT.
observed PWM frequency 38KHz at 19% duty cycle.

Why is controller not going back to PWM with frequency 90KHz when sync pwm is removed?
I can see peak voltage of RAMP is approximately 2.92V. In test case 1 &2, ramp peak voltage was 2.1V. why now ramp peak voltage has increased even though it is powered from Vref?
Schematic screen shot is as follows: