Part Number: UCC2897A
Other Parts Discussed in Thread: UCC2894
Hellow ,
I would like to design a offline power supply using forward converter topology.
The specifications are as follows
Input voltage: 280V to 330V
Output voltage: 100V
Power rating: 400W
Topology : Forward
IC:UCC2897A
I am thinking about the circuit diagram such as the chart below, is this constitution possible?
In addition, is it necessary to add diodes for rectification?

Thanks and Regards
Tomohiro Yoshimura