How can I separate the AGND and PGND when doing layout for TPS922055 / TPS922054 / TPS922053 / TPS922052 in VSON or SOT-23-THN package?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
If you want to separate the AGND and PGND for TPS922055 / TPS922054 / TPS922053 / TPS922052 in VSON or SOT-23-THN package, you can refer to the below layout example and its corresponding schematic for VSON package. Please pay attention to the single-point grounding connection between Pin1 (PGND) and Pin2 (AGND), which is represented by a 0Ω resistor in the schematic.
The layout for SOT-23-THN package is similar.