Other Parts Discussed in Thread: TPS922052, TPS922055, TPS922054, TPS922053
Is there a way to disable the thermal foldback function of TPS922055 / TPS922054 / TPS922053 / TPS922052 if I do not need this function?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
If the thermal foldback function is not needed (for example, if you want to exclude the influence of the thermal foldback function on the output current when you are doing the test), you can connect the TEMP pin to AGND pin to disable the thermal foldback function.