Other Parts Discussed in Thread: BQSTUDIO, , BQ76942
Greetings,
Out of ideas here.
Our BQ76942EVM board has been working previously but now after sitting on a table for about a month (until I got time to go at it again) I cannot seem to connect to it via BQStudio anymore, as if there's no communication via USB.
Usually I press WAKE button and I could connect through BQStudio. Now BQStudio won't detect the chip after pressing WAKE.
I'm using an actual 6-series-cell battery (26V) to connect to the EVM in such configuration on the EVM:
Measured some relevant signals:
TP2 BAT - 22.9V (correct for current SOC level).
TP3 CP1 - 33.7V (charge pump seems to work)
TP10 REG18 - 1.8V (REG 1.8V is functional once balancing cable is connected).
I was suspecting that perhaps chip is stuck in somekind of SLEEP mode.
I've exhausted some of the SLEEP mode topics here on the forum:
https://e2e.ti.com/support/power-management-group/power-management/f/power-management-forum/1273424/faq-bq76952-how-does-shutdown-mode-work?tisearch=e2e-sitesearch&keymatch=bq76952%2520faq
https://e2e.ti.com/support/power-management-group/power-management/f/power-management-forum/1273427/faq-bq76952-what-is-the-soft-shutdown-state
https://e2e.ti.com/support/power-management-group/power-management/f/power-management-forum/1181117/faq-bq76952-how-do-i-reset-the-bq769x2-device
One post refers to doing a partial reset by pressing RESET button. So I measured the relevant signals:
TP11 TS2 - 0.05V (floating) 0V when WAKE button held down.
- Perhaps multimeter may pull it low when trying to measure this?
TP7 REG1 - 0.618V
- REG1 has no significant output voltage to pull RST_SHUT up to !? Thus reset may not work at all...
BREG and REGIN are 0V
Are these levels expected ?
As of context, I have no other external circuitry attached to REG1 or TS2 pin.
I have also tried replacing the BQ76942 chip on the EVM, no change.
Connecting EVM via PSU and using the on-board cell simulation, only enables the FUSE LED and still no communication.
How would You suggest to go further to debug this ? As it worked some time before...