Other Parts Discussed in Thread: TPS74801
Hi team,
My customer faced an application of TPS54622 and TPS74801.
TPS74801 outputs the 2.5V and PowerGood, and TPS54622's EN pin is connected with the PowerGood pin of TPS74801.
Because the PowerGood pin of TPS75801 is an open-drain pin, my customer used a pull-up resistor (PR1 in the black-background schematic) at the TPS74801 side, and it is pulled-up to 3.3V.
At the same time, they added an extra pull-down resistor (PR2 in the black-background schematic) at the TPS54622 side.
My question is:
1. Is there any risk using this kind of circuit structure? Or does the values of these two resistors reasonable?
2. If the circuit structure or the values are not suitable, pls recommend any connection method between the TPS74801 (PG) and TPS54622 (EN),
Thanks a lot.
Customer's Application
The description of PG pin of TPS74801
PG pin of TPS74801