Other Parts Discussed in Thread: TPS61299
Hi TI Teams,
One of our customer reported that the efficiency is only 74%~76% with the real load like MCU,small fan and laser (the laser is switched on at 0.5s intervals, and the other loads run continuously). However, the efficiency is above 90% when tested with dummy loads. They also tried adding a 22uH Π filter circuit to the output, which would increase efficiency by 3%, but it didn't meet the requirements. The efficiency difference is only 3% with different inductors.
The schematic and layout is as below:


Do you have any good suggestion for this problem?
Thanks,
Kind Regards