This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5157-Q1: The sepic design tool of LM5157 of Cout

Part Number: LM5157-Q1


Here is the design value.

My design of the outout current is only 0.42A.

The output ripple of Vout is ±7.5%.

But the value of Cout is 32.25uF.

Cout = I * dt / dv = 0.42 * 0.385 / 440k / 0.15 = 2.45uF.

I think there is something wrong.