Other Parts Discussed in Thread: LMZ14203,
Hi,
I put the efuse tps16413 in the main input of my board.
there are few dc2dc in the board after the efuse.
the board have the followed currents:
constant current of about 100 mA + transient pulse of 250 mA in duration of 50 uSec on / 50 usec off.
The ISET is 1.5A.
the transient pulse get out from DC2DC LMZ14203.
the efuse tps1641 is turning off after few hours of work.
could it be issue of in to out short detection?
pls. advise
Zeev Gerber