Is there any graphical illustration about the transition of TPS922055 / TPS922054 / TPS922053 / TPS922052 from shutdown into hybrid dimming mode?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
The device will undergo two steps during the transition from shutdown to hybrid dimming mode. (Please keep ADIM/HD pin always low.)
Firstly, you need to follow the startup sequence shown in Section 8.3.4 and Figure 8-2 from the datasheet so that the device will be ready for dimming mode selection ("Dimming Mode Start" = high). The easiest way is to keep the EN/PWM pin high until the device is ready for dimming mode selection.
Secondly, you need to pull EN/PWM pin to low for a period of no shorter than 1us so that the device will enter into hybrid dimming mode. Then you can input your EN/PWM signal at the targeted duty and frequency. Please be noted that it takes 2 cycles for the device to detect the first targeted duty cycle after entering into hybrid dimming mode. Later it only takes 1 cycle to detect the targeted duty.
The TPS922055 / TPS922054 / TPS922053 / TPS922052 implements soft start feature to avoid inrush current during startup.
Please refer to the below graphical illustration.