Other Parts Discussed in Thread: TPS65987
Hi Team,
I have some questions about TPS65987D.
1) I only want to input 15V voltage to the device, but is it possible to set it to exclude other voltages?
For example, if a power supply that only supports up to 9V is input, such as a 25W adapter, is it possible to not input power to the device?
2) Is external Flash memory required in the circuit to set the PD required voltage to TPS65987?
Thanks,
Hiroki