Hello,
Can you please supply me with a noise density curve from 0.1Hz to 50MHz?
Thanks
Tom
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
Can you please supply me with a noise density curve from 0.1Hz to 50MHz?
Thanks
Tom
Hi Tom,
We have noise data for this device up to 100kHz, which is the maximum of the range it was designed around.
There is a plot in this article which shows the noise performance of this device, as well as the TPS7H1111-SP (our Ultra-Low Noise, High PSRR Radiation Hardened LDO).
Section 8.3.4 in the datasheet on Output Voltage Noise also shows a noise plot along with some additional details. Please note the different units used for the y-axis between these 2 sources.
Thanks,
Sarah