This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5164: Buck Converter working at lower voltages

Part Number: LM5164

Good Afternoon TI team,

We are looking for a buck converter, that can help provide a 10V output, with a variable input voltage of 22V - 58V. The LM5164 seems to be of interest.

However, I wanted to confirm it's operation at lower voltages. Let's say, we were to supply a voltage of 6V, would the LM5164 allow it to pass it as 6V (we are not looking for boosting it to 10V, just want to make sure it'll allow 6V to our load).

Thank you for your help.