This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC25600: Load regulation.

Part Number: UCC25600


Hi,

We are using UCC25600 for our project which is based of LLC. The system is designed to deliver an output power of 600W.

We are facing some issue in the load regulation of the system; the voltage is not stable; the output voltage keeps dipping during the load range.

The System rating is as below:

Vin: 320 -690 VAC

Vout1: 15V

Iout1:   20A

Vout2: 15V

Iout2 :15A

So, could you please help on this.

The schematic of the same is attached below.

LLC.pdf

Looking forward to your reply.

Regards,

Sreeni N K