Hi,
We are working with tps61288
and giving input 6V-8.4V lithium battery and Vout is =12V /2.5 amp
we have made the circuit in such a way that If the Vin falls below 6v the output turn off and when comes above 7.4V the output comes again ,this is controlled through a mosfet at the output of the boost convertor .
The problem we are facing here is once the mosfet is turned off that is the output disconnected when we increase the input voltage the boost IC is not reviving the voltage again .
if we do same process without output load that is through electronic load at 2.5 ampere the output comes above 7.4 and cuts below 6v.
Why is the boost ic not making voltage at load connected the voltage drops until we increase the voltage all the way upto to 8.4v.
Also please tell us the EN pin specifications .(its high logic voltage,disable low logic voltage and maximum voltage)
thanks