Other Parts Discussed in Thread: UCC27712
Hi, let's look at the following example using the LMG1205YFXT:
I have 5V between VDD and VSS and there are 80V between HS and VSS -> 75V between HS and VDD
These two pins are neighbours and IPC-2221B requires a clearance between the ball surface greater than 0.5mm. However the BGA pitch is 0.4mm, which means that the balls will have a clearance of ~0.2mm.
If there is a polymer coating of any kind, the requirement is only 0.13mm, so I conclude that the BGA package requires an underfill or a conformal coating to be used. I just want to know if that is the case or if I overlooked something.
So, do I need the coating to fulfill the requirements given in PCB and safety standards like the IPC-2221B or the IEC62368-1?
Thanks for your help