Other Parts Discussed in Thread: LM5069, TIDA-010242, LM74800-Q1
Hello Team,
i'm working through the datasheet and the APP-Note TIDA-010242. If i look at the schematic of MIL_STD_1275E_LM5069_Clamping_Circuit, i wonder about diode D1.
Can you clarify the function of the D1 in this circuit? At the moment i can only see a variation (amount of current on top) of calculated inrush current, because of 1µF capacitor belonging to the VS-Zener diode is charging via a path through Q1 D to S, through D1 to 1µF capacitor.
--------------------------------------------------------------------------------------------------------------------------------------------------------
Another thing is capacitor named "Ca". There are different values in the data sheet examples and the MIL-schematic
Data sheet figure 10-25 Ca=1µF
MIL-schematic: Ca=C8=0.015µF.
Is there any rule to calculate this capacitor, or how can i get the right value? From what parameters does it depend?
--------------------------------------------------------------------------------------------------------------------------------------------------------
And last but not least, is it right that LM74800-Q1 can block reverse current and LM74801-Q1 not, or is the only difference the way how they do it?
74800 with the help of linear regulation and 74801 with comparator?
Thanks a lot and best regards
Thomas