Hi, I am now thinking using UCC27611 as a gate driver for hull bridge inverter.
The input voltage is 200 V.
So, I made a gate drive circuit schematic in the Pspice for TI. And the simulation result showed that voltage potential about 200 V is applied to VDD, IN+, IN-, OUTPUT pins of high side UCC27611.
The UCC27611 is working properly because a potential difference is created on the high side for the UCC27611 to operate, but when viewed in terms of potential, the voltage is quite high on the pin. Will it break when actually used?
I attached the schematic and simulation result pdf. Please also check this.InverterDesign.pdfInverterResult.pdf
Sincerely,
Ryota Tauchi