Other Parts Discussed in Thread: TPS25750, TPS25751, TPS65987D, TPS65987DDK, TPS65987
Team,
what's the best single port alternative to TPS65994AD?
Best regards
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Team,
what's the best single port alternative to TPS65994AD?
Best regards
Hi Franziskus,
For single port solutions we have TPS65987D and TPS25750/1. TPS65987D supports PD power up to 100W (20V/5A) and alternate modes such as Display Port, TBT, and USB4. TPS25750 (and the next generation version which is TPS25751) only supports power-only application (no alternate mode support).
TPS65987D: https://www.ti.com/product/TPS65987D
TPS25751: https://www.ti.com/product/TPS25751
Thanks and Regards,
Raymond Lin
Hi Franziskus,
No problem, for additional support please open a new thread so we have better tracking!
Thanks and Regards,
Raymond Lin
Raymond,
I just checked the TPS65987D, and this device is only rated from -10°C to 75°C which is way too less since they need full -40 to 85°C temperature range.
The TPS25751 with no alternate mode is no alternative as well.
What about using TPS65994AD with just one port?
Does this make sense?
BR
Hi Franziskus,
The TPS65987DDK is going to have a larger operating temperature range (-40 to +85) so it should meet the customer's requirement. It also includes support for Alternate Modes such as Display Port and is a single-port PD.
Is this related to this e2e thread: https://e2e.ti.com/support/power-management-group/power-management/f/power-management-forum/1303543/tps65994ae-simple-1-port-dp-alt-mode-implementation
Thanks and Regards,
Raymond Lin
Raymond,
is the -40 to +85C support of TPS65987DDK coming soon?
Will this be a new device? ti.com does not reflect this.
Not sure if the posts are related., I am just covering for a colleague.
I read there is no timeline for the extended temp range.
I need a timeline to promote the device.
BR
Raymond,
adding feedback to my question above:
TPS65987DDK seems to be usable only for devices not for host ports.
Datasheet of TPS65987D seems to be the right of the family but it is -10-75°C.
BR
Hi Franziskus,
Currently we do not have a timeline for when TPS65987DDK will support the extended operating temperature range.
TPS65987D is configurable for both host and device platforms, configuration is done through the GUI tool that can be downloaded on the product page.
Thanks and Regards,
Raymond Lin
Raymond,
with that, I figure the only solution we have today is the TPS65994AD used with just one port.
Is there anything that needs to be considered when using the TPS65994AD with just one port.
BR
Hi Franziskus,
Please reach out to our product marketing team for more information on TPS65994AD. Due to holiday, responses may be delayed until January 2nd, 2024.
Thanks and Regards,
Raymond Lin