This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65313-Q1: sporadic reset after random time

Part Number: TPS65313-Q1

Team,
Can we please help with the below issue.
As first feedback I got the request to get the below additional information.
It will be added asap in this forum post:
    -To narrow down the issue what is the errors are seen just after reset?

    -Is there at first any CLOCK or ABIST errors showing up?


While analysing a problem in connection with your IC TPS65313-Q1, I came across the following forum entry:
https://e2e.ti.com/support/power-management-group/power-management/f/power-management-forum/1163109/tps65313-q1-reset-issue

The problem solution is unfortunately incomplete, but could provide important information for our error analysis.

In our case, the behaviour of the 3.3V and reset signal is similar to the forum entry listed. In practice, the behaviour manifests itself in a sporadic reset after a random time (~1h - 48h). Our implementation uses and triggers the watchdog and ESM, reads the available status information cyclically and an LBIST / ABIST is executed at regular intervals. The configuration of the
TPS is configured so that it switches to the safe state in the event of errors; only over/undervoltage at Buck1 are configured as reset errors (once in the safe state, the TPS actually remains in this state; the device error counter also does not lead to a reset in the current configuration). However, measurements do not show any over/undervoltages on the supply. The load is always <100mA.

Thanks in advance,
Anber