Hello TI,
I've found two issues with the Excel calculator for this device. Are there any plans to release an updated and corrected version?
The first is the current limit calculation of RILIM. Making Imax == 18.0 gives a suggested value of 67.94Ohm, but the calculator selects 124 Ohm for the actual, and will not allow me to over-ride. It complains about a value in G40, which is a blank cell.

The second issue is the VIN thresholds graph. The values are all completely nonsensical. Not a big deal, but I'm guessing it would be pretty easy to fix.

Thank You,
Ben