This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS1HC100-Q1: pin5 pin6

Part Number: TPS1HC100-Q1

May I ask how pins 5 and 6 should be configured?

  • Hi Ray,

    The LATCH pin can be left floating if auto retry is required. If the fault is to be latched, please pull the LATCH pin to logic level high through a pull up resistor.

    The SNS pin is to be connected to GND through a RSNS. This will allow the customer the ability to sense the output current using a ADC and MCU by converting the current through the device into a voltage on the SNS pin. 

    Please view the Application and Implementation section on the datasheet (Section 9) for more information.

    Thanks,

    Shreyas