Hello,
we want to implement with the driver IC UC3845 an flyback converter with isolated gate transformer to drive two mosfets of a big welding machine transformer.
The application is a welding machine with a transformator TR2.
I want to know what kind of driver IC I need to put on the primary side of the TR1 (gate drive transformer) in order to connect it to the UC3845:

Could you please also check if the secondary side of the Gate drive transformer is correct?
The Mosfets should be on at the same time.
regard Christian