This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello:
I have some questions in using the chip of LM1117MPX-5_0-NOPB.
Application case: input voltage = 9V,output voltage = 5V,load current = 150mA
Question's description:
(1)question1: After the device has been used for a period of time,the output of the chip appeared question as shown in figure below when load works.
(2)question2: After the device has been used for a period of time,the output voltage of the chip became 7V.
Hey masr,
Thanks a lot for reaching out.
Input and load conditions are well within the recommended limits only. Could you please provide details for input and output capacitor used in the circuit ?
Regards,
Rohit Phogat